Quarterly report pursuant to Section 13 or 15(d)

RECENTLY ADOPTED AND RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS

v2.3.0.15
RECENTLY ADOPTED AND RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS
9 Months Ended
Sep. 25, 2011
RECENTLY ADOPTED AND RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS  
RECENTLY ADOPTED AND RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS

NOTE 3.  RECENTLY ADOPTED AND RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS

 

Accounting Pronouncements Recently Adopted

 

In October 2009, the Financial Accounting Standards Board (FASB) amended its rules regarding the accounting for multiple element revenue arrangements.  The objective of the amendment is to allow vendors to account for revenue for different deliverables separately as opposed to part of a combined unit when those deliverables are provided at different times.  Specifically, this amendment addresses how to separate deliverables and simplifies the process of allocating revenue to the different deliverables when more than one deliverable exists.  The new rules were effective for us beginning January 1, 2011.  This amendment did not have a significant impact on our Condensed Consolidated Financial Statements as multiple element revenue arrangements are not material to our business.

 

Accounting Pronouncements Issued But Not Yet Effective

 

In September 2011, the FASB amended its standards related to the testing of goodwill for impairment.  The objective of this amendment is to simplify the annual goodwill impairment evaluation process.  The amendment provides entities the option to first assess qualitative factors to determine whether it is more likely than not that the fair value of a reporting unit is less than its carrying value as a basis for determining whether it is necessary to perform the two-step goodwill impairment test.  The two-step impairment test is now only required if an entity determines through this qualitative analysis that it is more likely than not that the fair value of the reporting unit is less than its carrying value.  The new rules will become effective during interim and annual periods beginning after December 15, 2011, however entities are permitted to early adopt the standard.  We plan to early adopt the standard and apply the qualitative analysis to certain reporting units in our 2011 goodwill impairment testing process.  Because the measurement of a potential impairment loss has not changed, the standard will not have a significant impact on our Consolidated Financial Statements.

 

In June 2011, the FASB amended its rules regarding the presentation of comprehensive income.  The objective of this amendment is to improve the comparability, consistency and transparency of financial reporting and to increase the prominence of items reported in other comprehensive income.  Specifically, this amendment requires that all non-owner changes in shareholders’ equity be presented either in a single continuous statement of comprehensive income or in two separate but consecutive statements.  In addition, the standard also requires disclosure of the location of reclassification adjustments between other comprehensive income and net income on the face of the financial statements.  The new rules are scheduled to become effective during interim and annual periods beginning after December 15, 2011.  The FASB recently added a project to its agenda to consider deferring certain aspects of this standard beyond the current anticipated effective date, specifically the provisions dealing with reclassification adjustments.  Because the standard only impacts the display of comprehensive income and does not impact what is included in comprehensive income, the standard will not have a significant impact on our Consolidated Financial Statements.

 

In May 2011, the FASB amended its standards related to fair value measurements and disclosures.  The objective of the amendment is to improve the comparability of fair value measurements presented and disclosed in financial statements prepared in accordance with U.S. GAAP and International Financial Reporting Standards.  Primarily, this amendment changed the wording used to describe many of the requirements in U.S. GAAP for measuring fair value and for disclosing information about fair value measurements in addition to clarifying the Board’s intent about the application of existing fair value measurement requirements.  The new standard also requires additional disclosures related to fair value measurements categorized within Level 3 of the fair value hierarchy and requires disclosure of the categorization in the hierarchy for items which are not recorded at fair value but fair value is required to be disclosed.  The new rules will become effective during interim and annual periods beginning after December 15, 2011.  As of September 25, 2011, we had no fair value measurements categorized within Level 3.  The only impact for us is expected to be the disclosure of the categorization in the fair value hierarchy for those items where fair value is only disclosed (primarily our debt obligations).