RECENTLY ADOPTED ACCOUNTING PRONOUNCEMENTS |
6 Months Ended |
|---|---|
Jun. 28, 2015 | |
| New Accounting Pronouncements and Changes in Accounting Principles [Abstract] | |
| RECENTLY ADOPTED ACCOUNTING PRONOUNCEMENTS |
NOTE 13. RECENTLY ISSUED ACCOUNTING PRONOUNCEMENTS
In May 2014, the FASB amended its standards related to revenue recognition. This amendment replaces all existing revenue recognition guidance and provides a single, comprehensive revenue recognition model for all contracts with customers. The standard contains principles that we will apply to determine the measurement of revenue and timing of when it is recognized. The underlying principle is that we will recognize revenue in a manner that depicts the transfer of goods or services to customers at an amount that we expect to be entitled to in exchange for those goods or services. The standard allows either full or modified retrospective adoption. The guidance provides a five-step analysis of transactions to determine when and how revenue is recognized. Other major provisions include capitalization of certain contract costs, consideration of time value of money in the transaction price and allowing estimates of variable consideration to be recognized before contingencies are resolved in certain circumstances. The amendment also requires additional disclosure about the nature, amount, timing and uncertainty of revenue and cash flows arising from customer contracts, including significant judgments and changes in judgments and assets recognized from costs incurred to fulfill a contract. The new rules would have become effective for annual and interim periods beginning January 1, 2017. In July 2015, the FASB approved a one year delay of the effective date of the standard to January 1, 2018, to provide adequate time for implementation, although the final amendment has not yet been published. We are in the process of evaluating the impact the amendment will have on our Consolidated Financial Statements, and we are further considering the impact of each method of adoption.
|