Cummins Center of Excellence for Oil and Gas Industry Opens in Houston
Two Centers of Excellence to Provide Integrated Power Packages for Oil and Gas Customers
HOUSTON--(BUSINESS WIRE)-- Cummins Inc. (NYSE: CMI) today announced the Cummins Oil and Gas Center of Excellence, a business launched to serve the needs of its growing oil and gas customer base. The Houston land-based center is located in a primary hub of engineering and technology for the oil and gas industry, and represents a significant investment by Cummins Inc. The Cummins Offshore Oil and Gas Center of Excellence is located in Singapore, geographically positioned in a global center of oil platform and shipbuilding and the home of related suppliers. Both facilities deliver a wide range of customized and integrated power packages specifically designed to the needs of each individual oil and gas customer.
"The Cummins Oil and Gas Center of Excellence allows Cummins to expand our current product offering beyond the broad range of diesel and natural gas engines currently available to customers," said Tom Linebarger, President and Chief Operating Officer. "What makes our Center of Excellence business model unique is our ability to provide customers with a complete integrated product designed to meet their unique needs. With the aid of our over 6,600 distributors and dealer locations globally, we are able to support this product wherever it goes around the world. The centers provide global technical sales support, design, testing and validation and package manufacturing and assembly. The final result is an integrated package delivering the superior performance and reliability that Cummins customers have come to expect."
Both operations will utilize Cummins standard work processes and procedures to perform design and validation testing of integrated equipment. The Houston center will deliver customized packages for the customer, starting with workover rigs capable of operating anywhere in the world, certified to the most stringent environmental regulations in California and other non-attainment regions - something no other engine manufacturer can provide. The center will also have the ability to integrate the new QTR Series Transmissions with our QSK50 or QSK60 engines, delivering a more integrated approach to working with customers. Other products include land-based drilling power modules, hazardous-area packages, pump drive packages and oil field power generator sets. Each system will be fully tested to Cummins standards, resulting in a quality product that meets customers exacting specifications. All complete customized products will be covered under Cummins warranty, and can be supported by more than 6,600 Cummins distributors and dealers worldwide.
The new Cummins Oil and Gas Center of Excellence will be fully operational at the end of June 2011 and will add 50 highly skilled jobs by the end of 2012, with future job growth expected in 2013. The new 70,000-square-foot building sits on six acres of land on the north side of Houston, and features office and meeting spaces, assembly cells, a paint booth and two test cells physically sized for up to a 78-liter engine. The two test cells with AVL instrumentation and testing system are capable of supporting both engineering and production testing and testing of mechanical or electrical drive systems up to 3500 hp (2610 kWe). The test facility is capable of conditioning the intake air up to 50 degrees Celsius for high ambient temperature testing, as well as supporting standard 23 degrees Celsius test conditions. All data is stored through a high-speed data acquisition system that ties directly into Cummins global test database.
"Cummins has chosen to locate the Oil and Gas Center of Excellence in Houston because we fully recognize that Houston is a major hub for business and engineering for the oil and gas market," said Carlos Ayala, General Manager - Center of Excellence Houston. "Because of the importance of the oil and gas business to Houston, there is an excellent source of industry resources. The Greater Houston Partnership Group and Harris County have played a large role in our decision to locate in Houston, providing incentives for skills development. We are also fortunate to expand upon our existing relationship with the University of Houston, allowing us to tap the university's resources for testing and foster a mentor program between our product engineers and students."
About Cummins Inc.
Cummins Inc., a global power leader, is a
corporation of complementary business units that design, manufacture,
distribute and service engines and related technologies, including fuel
systems, controls, air handling, filtration, emission solutions and
electrical power generation systems. Headquartered in Columbus, Indiana
(USA), Cummins employs approximately 40,000 people worldwide and serves
customers in approximately 190 countries and territories through a
network of more than 600 company-owned and independent distributor
locations and approximately 6,000 dealer locations. Cummins earned $1.0
billion on sales of $13.2 billion in 2010. Press releases can be found
on the Web at cummins.com or cumminsengines.com. Follow Cummins on
Twitter at http://twitter.com/cumminsengines
and YouTube at http://youtube.com/cumminsengines.
Source: Cummins Inc.
Released May 2, 2011