LEASES SUMMARY OF SIGNIFICANT ACCOUNTING POLICIES LEASES SUMMARY OF SIGNIFICANT ACCOUNTING POLICIES (Policies) |
6 Months Ended |
---|---|
Jun. 30, 2019 | |
Leases [Abstract] | |
Lessee, Leases - Policy |
We determine if an arrangement contains a lease in whole or in part at the inception of the contract. ROU assets represent our right to use an underlying asset for the lease term while lease liabilities represent our obligation to make lease payments arising from the lease. All leases greater than 12 months result in the recognition of a ROU asset and a liability at the lease commencement date based on the present value of the lease payments over the lease term. As most of our leases do not provide the information required to determine the implicit rate, we use our incremental borrowing rate based on the information available at commencement date in determining the present value of lease payments. This rate is determined considering factors such as the lease term, our credit standing and the economic environment of the location of the lease. We use the implicit rate when readily determinable.
Our lease terms include all non-cancelable periods and may include options to extend (or to not terminate) the lease when it is reasonably certain that we will exercise that option. Leases that have a term of 12 months or less at the commencement date are expensed on a straight-line basis over the lease term and do not result in the recognition of an asset or a liability.
Lease expense for operating leases is recognized on a straight-line basis over the lease term. Lease expense for finance leases are generally front-loaded as the finance lease ROU asset is depreciated on a straight-line basis, but interest expense on the liability is recognized utilizing the interest method that results in more expense during the early years of the lease. We have lease agreements with lease and non-lease components, primarily related to real estate, vehicle and Information Technology (IT) leases. For vehicle and real estate leases, we account for the lease and non-lease components as a single lease component. For IT leases, we allocate the payment between the lease and non-lease components based on the relative value of each component.
|